Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.ABSOLUTE
Interference solids positioned in absolute
coordinate system.
|
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.BOTH_SETS
Interference solids positioned relative to
interfering links in both sets.
|
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.FIRST_SET
Interference solids positioned relative to
interfering links in first set.
|
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.SECOND_SET
Interference solids positioned relative to
interfering links in second set.
|
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.SELECTED
Interference solids positioned relative to
user selected links.
|
Modifier and Type | Method and Description |
---|---|
PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.frameType()
Returns the
PackagingInterference frame type
defined at PackagingInterferenceBuilder.Frame
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingInterferenceBuilder.Frame |
PackagingInterferenceBuilder.Frame.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingInterferenceBuilder.Frame[] |
PackagingInterferenceBuilder.Frame.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PackagingInterferenceBuilder.setFrameType(PackagingInterferenceBuilder.Frame fType)
Sets the
PackagingInterference frame type
defined at PackagingInterferenceBuilder.Frame
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.