Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FlexBodyBuilder.Positioning |
FlexBodyBuilder.Positioning.ABSOLUTE_ORIGIN
Positioning to absolution place
|
static FlexBodyBuilder.Positioning |
FlexBodyBuilder.Positioning.COMPONENT_POSITION
Positioning to the place where the component is in assembly
|
static FlexBodyBuilder.Positioning |
FlexBodyBuilder.Positioning.THREE_POINT_METHOD
Positioning to user defined place using three point method
|
Modifier and Type | Method and Description |
---|---|
FlexBodyBuilder.Positioning |
FlexBodyBuilder.positioningType()
Returns the positioning type
License requirements: None. |
static FlexBodyBuilder.Positioning |
FlexBodyBuilder.Positioning.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexBodyBuilder.Positioning |
FlexBodyBuilder.Positioning.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexBodyBuilder.Positioning[] |
FlexBodyBuilder.Positioning.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlexBodyBuilder.setPositioningType(FlexBodyBuilder.Positioning positioningType)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.