Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DriverOperation.IntegrationType |
DriverOperation.IntegrationType.ACCELERATION
Acceleration
|
static DriverOperation.IntegrationType |
DriverOperation.IntegrationType.DISPLACEMENT
Displacement
|
static DriverOperation.IntegrationType |
DriverOperation.IntegrationType.VELOCITY
Velocity
|
Modifier and Type | Method and Description |
---|---|
DriverOperation.IntegrationType |
DriverOperation.integrationTypeOption()
Returns the integration type option
License requirements: None. |
static DriverOperation.IntegrationType |
DriverOperation.IntegrationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DriverOperation.IntegrationType |
DriverOperation.IntegrationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DriverOperation.IntegrationType[] |
DriverOperation.IntegrationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DriverOperation.setIntegrationTypeOption(DriverOperation.IntegrationType integrationTypeOption)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.