Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CurveParameterizedTypes |
CurveParameterizedTypes.CURVATURE
Curvature based type
|
static CurveParameterizedTypes |
CurveParameterizedTypes.SPACING
User defined spacing type
|
Modifier and Type | Method and Description |
---|---|
CurveParameterizedTypes |
PointOnCurveBuilder.curveParameterizedType()
Returns the curve parameterized type
License requirements: None. |
static CurveParameterizedTypes |
CurveParameterizedTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveParameterizedTypes |
CurveParameterizedTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveParameterizedTypes[] |
CurveParameterizedTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PointOnCurveBuilder.setCurveParameterizedType(CurveParameterizedTypes curveParameterizedType)
License requirements: mechanisms ("MECHANISMS") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.