Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CouplerCable
Represents a motion cable object
To create or edit an instance of this class, use CouplerCableBuilder Created in NX6.0.0 |
interface |
CouplerGear
Represents a motion gear object
To create or edit an instance of this class, use CouplerGearBuilder Created in NX6.0.0 |
interface |
CouplerRckpn
Represents a motion rack and pinion object
To create or edit an instance of this class, use CouplerRckpnBuilder Created in NX6.0.0 |
Modifier and Type | Method and Description |
---|---|
Coupler |
CouplerCollection.findObject(String name)
Finds a coupler with the given name.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.