Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static SignalAdapterBuilder.DataPortType |
SignalAdapterBuilder.DataPortType.INPUT
Input
|
static SignalAdapterBuilder.DataPortType |
SignalAdapterBuilder.DataPortType.OUTPUT
Output
|
SignalAdapterBuilder.DataPortType |
SignalAdapterBuilder.SignalData.portType
Data Port Type
|
Modifier and Type | Method and Description |
---|---|
static SignalAdapterBuilder.DataPortType |
SignalAdapterBuilder.DataPortType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SignalAdapterBuilder.DataPortType |
SignalAdapterBuilder.DataPortType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SignalAdapterBuilder.DataPortType[] |
SignalAdapterBuilder.DataPortType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
SignalData(String nameInitial,
SignalAdapterBuilder.DataType dataTypeInitial,
SignalAdapterBuilder.DataPortType portTypeInitial,
boolean boolValueInitial,
int intValueInitial,
double doubleValueInitial,
Unit unitInitial,
int signalIdInitial,
AdapterSignal editedSignalInitial,
AdapterFormula assignedFormulaInitial,
String formulaInitial,
String commentInitial)
Constructor for the SignalData object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.