Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.SlaveValueUnit.LINEAR_POSITION
Linear Position
|
static GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.SlaveValueUnit.LINEAR_SPEED
Linear Speed
|
static GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.SlaveValueUnit.ROTARY_POSITION
Rotary Position
|
static GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.SlaveValueUnit.ROTARY_SPEED
Rotary Speed
|
Modifier and Type | Method and Description |
---|---|
GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.slaveUnit()
Returns the slave value unit
License requirements: None. |
static GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.SlaveValueUnit.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GraphControlBuilder.SlaveValueUnit |
GraphControlBuilder.SlaveValueUnit.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GraphControlBuilder.SlaveValueUnit[] |
GraphControlBuilder.SlaveValueUnit.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GraphControlBuilder.setSlaveUnit(GraphControlBuilder.SlaveValueUnit slaveType)
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.