Interface | Description |
---|---|
Circle |
Represents a
nxopen.Markup.Circle
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createCircle Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
EditObjectDisplayBuilder |
The
nxopen.Markup.EditObjectDisplayBuilder is used to edit display settings of the markup objects. |
Ellipse |
Represents a
nxopen.Markup.Ellipse
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createEllipse Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
File |
Represents a
nxopen.Markup.File
To create a new instance of this class, use nxopen.Markup.MarkupFileCollection#createFile Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Freehand |
Represents a
nxopen.Markup.Freehand
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createFreehand Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Icon |
Represents a
nxopen.Markup.Icon
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createIcon Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
MarkupFileCollection |
Represents a
nxopen.Markup.MarkupFileCollection To obtain an instance of this class, refer to nxopen.Markup.MarkupManager Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
MarkupFileObjectCollection |
This collects all the markups in the
nxopen.Markup.File To obtain an instance of this class, refer to nxopen.Markup.File Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
MarkupManager |
Contains the collection objects for creating and iterating over markup objects.
|
MarkupObject |
Represents a
nxopen.Markup.MarkupObject on the screen. |
MarkupObjectCollection |
This collects all the markups in current NX session
To obtain an instance of this class, refer to nxopen.Markup.MarkupManager Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Polyline |
Represents a
nxopen.Markup.Polyline
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createPolyline Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Rectangle |
Represents a
nxopen.Markup.Rectangle
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createRectangle Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Text |
Represents a
nxopen.Markup.Text
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createText Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Class | Description |
---|---|
Circle.CenterAndRadiusData |
This class holds the data returned from
Circle.getCenterAndRadius() |
Ellipse.CenterAndRadiusData |
This class holds the data returned from
Ellipse.getCenterAndRadius() |
Icon.Size |
Represents the possible
nxopen.Markup.Icon size. |
Polyline.LineOption |
Represents the
nxopen.Markup.Polyline line option. |
Rectangle.CenterLengthAndWidthData |
This class holds the data returned from
Rectangle.getCenterLengthAndWidth() |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.