Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.issue |
Provides classes and interfaces for the Issue Management.
|
Class and Description |
---|
IssueManager
Contains the collection objects for creating and iterating over issue objects.
|
Class and Description |
---|
IssueAttachment
Represents the Issue Attachment object.
|
IssueContent
Represents the Issue Issue object.
|
IssueFolder
Represents the Issue Folder object.
|
IssueList
Represents the Issue List object.
|
IssueSite
Represents the Issue Site object.
|
Class and Description |
---|
IssueAttachment
Represents the Issue Attachment object.
|
IssueAttachment.Type
Represents the possible attachment types
for a
IssueAttachment . |
IssueBriefcase
Represents the Issue Briefcase object.
|
IssueBriefcaseSynchronizeBuilder
Represents a
IssueBriefcase synchronize builder To create a new instance of this class, use IssueBriefcase.createSynchronizeContentBuilder() Created in NX10.0.0 |
IssueContent
Represents the Issue Issue object.
|
IssueContent.IsCheckedOutData
This class holds the data returned from
IssueContent.isCheckedOut() |
IssueContentBuilder
Represents a
IssueContent builder To create a new instance of this class, use IssueManager.createIssueContentBuilder(nxopen.issue.IssueContent) Default values. |
IssueFolder
Represents the Issue Folder object.
|
IssueFolder.Type
Represents the possible folder types
for a
IssueFolder . |
IssueList
Represents the Issue List object.
|
IssueListCollection
Represents a
IssueListCollection To obtain an instance of this class, refer to IssueManager Created in NX8.5.0 |
IssueManager.Mode
Represents the possible issue site modes.
|
IssueManager.State
Represents the possible issue object states.
|
IssueProperty
Represents the Issue Property object.
|
IssueProperty.Type
Represents the possible property types.
|
IssueSite
Represents the Issue Site object.
|
SnapshotSubsetBuilder
Used to create or edit issue snapshot subset.
|
SnapshotSubsetBuilder.ContextType
The option specifying which kinds of issue snapshot subset should be created.
|
SnapshotWorksetBuilder
Used to create or edit issue snapshot workset which is a container to hold all the corresponding
parts to represent an issue.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.