Interface | Description |
---|---|
IssueAttachment |
Represents the Issue Attachment object.
|
IssueBriefcase |
Represents the Issue Briefcase object.
|
IssueBriefcaseSynchronizeBuilder |
Represents a
IssueBriefcase synchronize builder To create a new instance of this class, use IssueBriefcase.createSynchronizeContentBuilder() Created in NX10.0.0 |
IssueContent |
Represents the Issue Issue object.
|
IssueContentBuilder |
Represents a
IssueContent builder To create a new instance of this class, use IssueManager.createIssueContentBuilder(nxopen.issue.IssueContent) Default values. |
IssueFolder |
Represents the Issue Folder object.
|
IssueList |
Represents the Issue List object.
|
IssueListCollection |
Represents a
IssueListCollection To obtain an instance of this class, refer to IssueManager Created in NX8.5.0 |
IssueManager |
Contains the collection objects for creating and iterating over issue objects.
|
IssueProperty |
Represents the Issue Property object.
|
IssueSite |
Represents the Issue Site object.
|
SnapshotSubsetBuilder |
Used to create or edit issue snapshot subset.
|
SnapshotWorksetBuilder |
Used to create or edit issue snapshot workset which is a container to hold all the corresponding
parts to represent an issue.
|
Class | Description |
---|---|
IssueAttachment.Type |
Represents the possible attachment types
for a
IssueAttachment . |
IssueContent.IsCheckedOutData |
This class holds the data returned from
IssueContent.isCheckedOut() |
IssueFolder.Type |
Represents the possible folder types
for a
IssueFolder . |
IssueManager.Mode |
Represents the possible issue site modes.
|
IssueManager.State |
Represents the possible issue object states.
|
IssueProperty.Type |
Represents the possible property types.
|
SnapshotSubsetBuilder.ContextType |
The option specifying which kinds of issue snapshot subset should be created.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.