Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
FtmTransformCurvesBuilder |
OmnicadManager.createFtmTransformCurvesBuilder()
Creates Free Transformer transform curves builder.
|
FtmTransformCurvesBuilder |
FtmTransformCurvesBuilderList.findItem(int index)
Returns the object at the input index.
|
FtmTransformCurvesBuilder[] |
FtmTransformCurvesBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FtmTransformCurvesBuilderList.append(FtmTransformCurvesBuilder object)
Appends an object to the list
License requirements: None. |
void |
FtmTransformCurvesBuilderList.append(FtmTransformCurvesBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FtmTransformCurvesBuilderList.erase(FtmTransformCurvesBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
FtmTransformCurvesBuilderList.erase(FtmTransformCurvesBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FtmTransformCurvesBuilderList.findIndex(FtmTransformCurvesBuilder obj)
Finds the index where the input object appears.
|
void |
FtmTransformCurvesBuilderList.insert(int location,
FtmTransformCurvesBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
FtmTransformCurvesBuilderList.setContents(FtmTransformCurvesBuilder[] objects)
Sets the contents of the entire list.
|
void |
FtmTransformCurvesBuilderList.swap(FtmTransformCurvesBuilder object1,
FtmTransformCurvesBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.