Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
FaceSetOffset |
OffsetSurfaceBuilder.findFaceSet(int index)
Deprecated.
Deprecated in NX5.0.0. Use
OffsetSurfaceBuilder.faceSets() instead.
|
FaceSetOffset[] |
OffsetSurfaceBuilder.getFaceSets()
Deprecated.
Deprecated in NX5.0.0. Use
OffsetSurfaceBuilder.faceSets() instead.
|
Modifier and Type | Method and Description |
---|---|
void |
OffsetSurfaceBuilder.addFaceSets(FaceSetOffset[] faceSets)
Deprecated.
Deprecated in NX5.0.0. Use
OffsetSurfaceBuilder.faceSets() instead.
|
Modifier and Type | Method and Description |
---|---|
FaceSetOffset |
FaceSetOffsetCollection.createEmptyFaceSet()
Creates an empty offset face set, with all parameters set to 0 or null
License requirements: solid_modeling ("SOLIDS MODELING") . |
FaceSetOffset |
FaceSetOffsetCollection.createFaceSet(String offset,
ScCollector faceCollector,
boolean flipValue,
int index)
Creates an offset face set.
|
FaceSetOffset |
FaceSetOffsetList.findItem(int index)
Returns the object at the input index.
|
FaceSetOffset[] |
FaceSetOffsetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FaceSetOffsetList.append(FaceSetOffset object)
Appends an object to the list
License requirements: None. |
void |
FaceSetOffsetList.append(FaceSetOffset[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FaceSetOffsetList.erase(FaceSetOffset obj)
Erases the object from the list, but does not delete the object.
|
void |
FaceSetOffsetList.erase(FaceSetOffset obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FaceSetOffsetList.findIndex(FaceSetOffset obj)
Finds the index where the input object appears.
|
void |
FaceSetOffsetList.insert(int location,
FaceSetOffset object)
Inserts an object at the specified location
License requirements: None. |
void |
FaceSetOffsetList.setContents(FaceSetOffset[] objects)
Sets the contents of the entire list.
|
void |
FaceSetOffsetList.swap(FaceSetOffset object1,
FaceSetOffset object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.