public class Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO_OFFSET
No offset
|
static int |
_NONSYMMETRIC_OFFSET
Offset with two different distances
|
static int |
_SINGLE_OFFSET
Offset with single distance in one direction
|
static int |
_SYMMETRIC_OFFSET
Offset with same distance in both directions
|
static Type |
NO_OFFSET
No offset
|
static Type |
NONSYMMETRIC_OFFSET
Offset with two different distances
|
static Type |
SINGLE_OFFSET
Offset with single distance in one direction
|
static Type |
SYMMETRIC_OFFSET
Offset with same distance in both directions
|
Modifier and Type | Method and Description |
---|---|
static Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final Type NO_OFFSET
public static final Type NONSYMMETRIC_OFFSET
public static final Type SYMMETRIC_OFFSET
public static final Type SINGLE_OFFSET
public static final int _NO_OFFSET
public static final int _NONSYMMETRIC_OFFSET
public static final int _SYMMETRIC_OFFSET
public static final int _SINGLE_OFFSET
public static Type valueOf(int value)
public static Type valueOf(String name)
public static Type[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.