public static class SupportPlaneData.LockPlaneStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AFTER_ALL_CONSTRAINT
Lock after all constraint
|
static int |
_AFTER_FIRST_AND_SECOND_CONSTRAINT
Lock after first and second constraint
|
static int |
_AFTER_FIRST_AND_THIRD_CONSTRAINT
Lock after first and third constraint
|
static int |
_AFTER_FIRST_CONSTRAINT
Lock after first constraint
|
static int |
_AFTER_SECOND_AND_THIRD_CONSTRAINT
Lock after second and third constraint
|
static int |
_AFTER_SECOND_CONSTRAINT
Lock after second constraint
|
static int |
_AFTER_THIRD_CONSTRAINT
Lock after third constraint
|
static int |
_CENTER_POINT_DIRECTION
Lock support plane using center point and direction, this option should be used for Center Radius Arc only
|
static int |
_LOCK_EXISTING_PLANE
Lock support plane using existing face or datum
|
static int |
_NO
No Lock
|
static SupportPlaneData.LockPlaneStatus |
AFTER_ALL_CONSTRAINT
Lock after all constraint
|
static SupportPlaneData.LockPlaneStatus |
AFTER_FIRST_AND_SECOND_CONSTRAINT
Lock after first and second constraint
|
static SupportPlaneData.LockPlaneStatus |
AFTER_FIRST_AND_THIRD_CONSTRAINT
Lock after first and third constraint
|
static SupportPlaneData.LockPlaneStatus |
AFTER_FIRST_CONSTRAINT
Lock after first constraint
|
static SupportPlaneData.LockPlaneStatus |
AFTER_SECOND_AND_THIRD_CONSTRAINT
Lock after second and third constraint
|
static SupportPlaneData.LockPlaneStatus |
AFTER_SECOND_CONSTRAINT
Lock after second constraint
|
static SupportPlaneData.LockPlaneStatus |
AFTER_THIRD_CONSTRAINT
Lock after third constraint
|
static SupportPlaneData.LockPlaneStatus |
CENTER_POINT_DIRECTION
Lock support plane using center point and direction, this option should be used for Center Radius Arc only
|
static SupportPlaneData.LockPlaneStatus |
LOCK_EXISTING_PLANE
Lock support plane using existing face or datum
|
static SupportPlaneData.LockPlaneStatus |
NO
No Lock
|
Modifier and Type | Method and Description |
---|---|
static SupportPlaneData.LockPlaneStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SupportPlaneData.LockPlaneStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SupportPlaneData.LockPlaneStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final SupportPlaneData.LockPlaneStatus NO
public static final SupportPlaneData.LockPlaneStatus AFTER_FIRST_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus AFTER_SECOND_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus AFTER_THIRD_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus AFTER_FIRST_AND_SECOND_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus AFTER_FIRST_AND_THIRD_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus AFTER_SECOND_AND_THIRD_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus AFTER_ALL_CONSTRAINT
public static final SupportPlaneData.LockPlaneStatus LOCK_EXISTING_PLANE
public static final SupportPlaneData.LockPlaneStatus CENTER_POINT_DIRECTION
public static final int _NO
public static final int _AFTER_FIRST_CONSTRAINT
public static final int _AFTER_SECOND_CONSTRAINT
public static final int _AFTER_THIRD_CONSTRAINT
public static final int _AFTER_FIRST_AND_SECOND_CONSTRAINT
public static final int _AFTER_FIRST_AND_THIRD_CONSTRAINT
public static final int _AFTER_SECOND_AND_THIRD_CONSTRAINT
public static final int _AFTER_ALL_CONSTRAINT
public static final int _LOCK_EXISTING_PLANE
public static final int _CENTER_POINT_DIRECTION
public static SupportPlaneData.LockPlaneStatus valueOf(int value)
public static SupportPlaneData.LockPlaneStatus valueOf(String name)
public static SupportPlaneData.LockPlaneStatus[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.