Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static HighlightLinesAnalysisBuilder.Types |
HighlightLinesAnalysisBuilder.Types.BETWEEN_POINTS
Deprecated.
Between Points: Two highlight lines are guaranteed to
pass through two given surface points.
|
static HighlightLinesAnalysisBuilder.Types |
HighlightLinesAnalysisBuilder.Types.THROUGH_POINTS
Deprecated.
Through Points: A highlight line is guaranteed to pass through a surface point.
|
static HighlightLinesAnalysisBuilder.Types |
HighlightLinesAnalysisBuilder.Types.UNIFORM
Deprecated.
Uniform: Lights are placed uniformly on light plane
|
Modifier and Type | Method and Description |
---|---|
HighlightLinesAnalysisBuilder.Types |
HighlightLinesAnalysisBuilder.type()
Deprecated.
|
static HighlightLinesAnalysisBuilder.Types |
HighlightLinesAnalysisBuilder.Types.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static HighlightLinesAnalysisBuilder.Types |
HighlightLinesAnalysisBuilder.Types.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static HighlightLinesAnalysisBuilder.Types[] |
HighlightLinesAnalysisBuilder.Types.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HighlightLinesAnalysisBuilder.setType(HighlightLinesAnalysisBuilder.Types type)
Deprecated.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.