Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static GeometricProperties.OutputType |
GeometricProperties.OutputType.DYNAMIC
Properties of an entity are displayed first on the dialog
itself on mouse over.
|
static GeometricProperties.OutputType |
GeometricProperties.OutputType.STATIC
Propeties of the selected entities are displayed in the
information window.
|
Modifier and Type | Method and Description |
---|---|
GeometricProperties.OutputType |
GeometricProperties.outputMethod()
Returns the output method
License requirements: None. |
static GeometricProperties.OutputType |
GeometricProperties.OutputType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricProperties.OutputType |
GeometricProperties.OutputType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricProperties.OutputType[] |
GeometricProperties.OutputType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeometricProperties.setOutputMethod(GeometricProperties.OutputType outputMethod)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.