nxopen.geometricanalysis.HighlightLinesAnalysisBuilder#lightPlacements
and nxopen.geometricanalysis.HighlightLinesAnalysisBuilder#setLightPlacements
instead.
public static class HighlightLinesAnalysisBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BETWEEN_POINTS
Deprecated.
Between Points: Two highlight lines are guaranteed to
pass through two given surface points.
|
static int |
_THROUGH_POINTS
Deprecated.
Through Points: A highlight line is guaranteed to pass through a surface point.
|
static int |
_UNIFORM
Deprecated.
Uniform: Lights are placed uniformly on light plane
|
static HighlightLinesAnalysisBuilder.Types |
BETWEEN_POINTS
Deprecated.
Between Points: Two highlight lines are guaranteed to
pass through two given surface points.
|
static HighlightLinesAnalysisBuilder.Types |
THROUGH_POINTS
Deprecated.
Through Points: A highlight line is guaranteed to pass through a surface point.
|
static HighlightLinesAnalysisBuilder.Types |
UNIFORM
Deprecated.
Uniform: Lights are placed uniformly on light plane
|
Modifier and Type | Method and Description |
---|---|
static HighlightLinesAnalysisBuilder.Types |
valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static HighlightLinesAnalysisBuilder.Types |
valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static HighlightLinesAnalysisBuilder.Types[] |
values()
Deprecated.
Returns an array that contains the values for this enum.
|
public static final HighlightLinesAnalysisBuilder.Types UNIFORM
public static final HighlightLinesAnalysisBuilder.Types THROUGH_POINTS
public static final HighlightLinesAnalysisBuilder.Types BETWEEN_POINTS
public static final int _UNIFORM
public static final int _THROUGH_POINTS
public static final int _BETWEEN_POINTS
public static HighlightLinesAnalysisBuilder.Types valueOf(int value)
public static HighlightLinesAnalysisBuilder.Types valueOf(String name)
public static HighlightLinesAnalysisBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.