public static class ImageCaptureBuilder.CaptureMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FILE
the input from file
|
static int |
_GRAPHICS_AREA
the graphics area
|
static int |
_REGION
the region area
|
static ImageCaptureBuilder.CaptureMethodType |
FILE
the input from file
|
static ImageCaptureBuilder.CaptureMethodType |
GRAPHICS_AREA
the graphics area
|
static ImageCaptureBuilder.CaptureMethodType |
REGION
the region area
|
Modifier and Type | Method and Description |
---|---|
static ImageCaptureBuilder.CaptureMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImageCaptureBuilder.CaptureMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImageCaptureBuilder.CaptureMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ImageCaptureBuilder.CaptureMethodType GRAPHICS_AREA
public static final ImageCaptureBuilder.CaptureMethodType REGION
public static final ImageCaptureBuilder.CaptureMethodType FILE
public static final int _GRAPHICS_AREA
public static final int _REGION
public static final int _FILE
public static ImageCaptureBuilder.CaptureMethodType valueOf(int value)
public static ImageCaptureBuilder.CaptureMethodType valueOf(String name)
public static ImageCaptureBuilder.CaptureMethodType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.