Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Method and Description |
---|---|
PathObjects |
FieldManager.createPathObjects()
Creates a
PathObjects
License requirements: None. |
PathObjects |
PathObjectsList.findItem(int index)
Returns the object at the input index.
|
PathObjects[] |
PathObjectsList.getContents()
Gets the contents of the entire list
License requirements: None. |
PathObjects |
SpatialMapBuilder.latticePath()
Returns the lattice path objects
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PathObjectsList.append(PathObjects object)
Appends an object to the list
License requirements: None. |
void |
PathObjectsList.append(PathObjects[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PathObjectsList.erase(PathObjects obj)
Erases the object from the list, but does not delete the object.
|
void |
PathObjectsList.erase(PathObjects obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PathObjectsList.findIndex(PathObjects obj)
Finds the index where the input object appears.
|
void |
PathObjectsList.insert(int location,
PathObjects object)
Inserts an object at the specified location
License requirements: None. |
void |
PathObjectsList.setContents(PathObjects[] objects)
Sets the contents of the entire list.
|
void |
PathObjectsList.swap(PathObjects object1,
PathObjects object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.