Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ResultProbe
Result Probe Object.
|
Modifier and Type | Interface and Description |
---|---|
interface |
FieldExpression
Represents the Field Expression class.
|
interface |
FieldFormula
Represents the Field Formula class.
|
interface |
FieldLink
Represents the Field Link class.
|
interface |
FieldReference
Represents an reference field
A Reference Field exposes data inside of an abstract data store. |
Modifier and Type | Method and Description |
---|---|
Field |
Field.createCopyInPart(BasePart targetPart)
Copy the field to the target part.
|
Field |
FieldManager.deleteField(Field field)
Deletes the specified
Field object; if the object cannot be deleted
it is returned. |
Field |
VectorFieldWrapper.getField()
Returns the implementation if the wrapper is backed up by a field;
NULL otherwise
License requirements: None. |
Field |
ScalarFieldWrapper.getField()
Returns the implementation if the wrapper is backed up by a field;
NULL otherwise
License requirements: None. |
Field |
FieldWrapper.getField()
Returns the implementation
License requirements: None. |
Field[] |
ImportData.getFields()
Return the fields that have been imported
License requirements: None. |
Field[] |
ExportData.getFields()
Gets the fields
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ExportData.addField(Field field)
Add a field
License requirements: None. |
void |
ExportData.addFields(Field[] fields)
Add a field
License requirements: None. |
FieldVariable |
FieldManager.createDependentVariable(Field ownerField,
NameVariable nameVariable,
Unit unitType)
Create a dependent variable to be added to the field
License requirements: None. |
DisplayPropertiesBuilder |
FieldManager.createDisplayPropertiesBuilder(Field[] fieldArray)
Creates a
DisplayPropertiesBuilder
License requirements: None. |
FieldLink |
FieldManager.createFieldLink(String fieldName,
Field fieldToLink)
Creates a
FieldLink . |
FieldLinksTable |
FieldManager.createFieldLinksTable(String fieldName,
FieldVariable[] indepVarArray,
FieldVariable[] depVarArray,
double[] datapoints,
Field[] linkFieldsArray)
Creates a
nxopen.fields.FieldLinksTable object with dependent and independent variables
FieldVariable . |
FieldWrapper |
FieldManager.createFieldWrapper(Field field)
Create a field wrapper backed up by a field
License requirements: None. |
FieldVariable |
FieldManager.createIndependentVariable(Field ownerField,
NameVariable nameVariable,
Unit unitType,
boolean minValueSet,
boolean minValueInclusive,
double minValue,
boolean maxValueSet,
boolean maxValueInclusive,
double maxValue,
boolean numPtsSet,
int numPts,
boolean defaultValueSet,
double defaultValue)
Create an independent variable to be added to the field
License requirements: None. |
ScalarFieldWrapper |
FieldManager.createScalarFieldWrapperWithField(Field field,
double scaleFactor)
Create a scalar field wrapper backed up by a scaled scalar field
License requirements: None. |
VectorFieldWrapper |
FieldManager.createVectorFieldWrapperWithField(Field field,
double[] scaleFactors)
Create a vector field wrapper backed up by a scaled vector field
License requirements: None. |
Field |
FieldManager.deleteField(Field field)
Deletes the specified
Field object; if the object cannot be deleted
it is returned. |
void |
FieldLink.editFieldLink(Field fieldToLink)
Edit the link field.
|
void |
FieldWrapper.setField(Field field)
Sets the implementation of the wrapper to the specified field
License requirements: None. |
void |
ScalarFieldWrapper.setField(Field field,
double scaleFactor)
Sets the implementation of the wrapper to the specified field
License requirements: None. |
void |
VectorFieldWrapper.setField(Field field,
double[] scaleFactors)
Sets the implementation of the wrapper to the specified field
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.