public interface VectorFieldWrapper extends NXObject
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat
Modifier and Type | Method and Description |
---|---|
Expression |
getExpressionByIndex(int index)
Returns the indicated implementation if the wrapper is backed up by expressions;
NULL otherwise
License requirements: None. |
Field |
getField()
Returns the implementation if the wrapper is backed up by a field;
NULL otherwise
License requirements: None. |
void |
setExpressions(Expression[] expressions)
Sets the implementation of the wrapper to the specified expressions
License requirements: None. |
void |
setField(Field field,
double[] scaleFactors)
Sets the implementation of the wrapper to the specified field
License requirements: None. |
deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void setExpressions(Expression[] expressions) throws NXException, RemoteException
expressions
- existing expressions that will be this wrapper's valueNXException
RemoteException
Expression getExpressionByIndex(int index) throws NXException, RemoteException
index
- 0, 1 or 2NXException
RemoteException
void setField(Field field, double[] scaleFactors) throws NXException, RemoteException
field
- an existing field that will be this wrapper's valuescaleFactors
- the field will be multiplied by this scale factor when being evaluatedNXException
RemoteException
Field getField() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.