public interface FieldVariable extends NXObject
Unit
). Modifier and Type | Interface and Description |
---|---|
static class |
FieldVariable.Bounds
Variable Bounds structure
|
static class |
FieldVariable.Type
Variable Types
|
static class |
FieldVariable.ValueType
Variable value Type
|
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat
Modifier and Type | Method and Description |
---|---|
double |
defaultValue()
Returns the variable's default value which is value used when evaluating a field and no value is specified
License requirements: None. |
boolean |
logarithmic()
Returns the flag indicating if the units for this variable are stored/retrieved as logarithmic units
License requirements: None. |
NameVariable |
nameVariable()
Returns the name variable for this variable.
|
int |
numPoints()
Returns the number of points used for this variable when generating a table
License requirements: None. |
Unit |
units()
Returns the units for this variable, which can be null if the variable is unitless.
|
FieldVariable.Bounds |
variableBounds()
Returns the variable's minimum and maximum bounds.
|
FieldVariable.Type |
variableType()
Returns the type of variable.
|
deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
Unit units() throws NXException, RemoteException
NXException
RemoteException
NameVariable nameVariable() throws NXException, RemoteException
NXException
RemoteException
FieldVariable.Type variableType() throws NXException, RemoteException
NXException
RemoteException
FieldVariable.Bounds variableBounds() throws NXException, RemoteException
NXException
RemoteException
double defaultValue() throws NXException, RemoteException
NXException
RemoteException
int numPoints() throws NXException, RemoteException
NXException
RemoteException
boolean logarithmic() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.