Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static WindshieldDatumBuilder.EnumEyeType |
WindshieldDatumBuilder.EnumEyeType.EYE_FEATURE
eye feature
|
static WindshieldDatumBuilder.EnumEyeType |
WindshieldDatumBuilder.EnumEyeType.V1POINT
v1 point
|
static WindshieldDatumBuilder.EnumEyeType |
WindshieldDatumBuilder.EnumEyeType.V2POINT
v2 point
|
Modifier and Type | Method and Description |
---|---|
WindshieldDatumBuilder.EnumEyeType |
WindshieldDatumBuilder.eyeType()
Returns the eye type to determine which type of v points to be used.
|
static WindshieldDatumBuilder.EnumEyeType |
WindshieldDatumBuilder.EnumEyeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WindshieldDatumBuilder.EnumEyeType |
WindshieldDatumBuilder.EnumEyeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WindshieldDatumBuilder.EnumEyeType[] |
WindshieldDatumBuilder.EnumEyeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WindshieldDatumBuilder.setEyeType(WindshieldDatumBuilder.EnumEyeType eyeType)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.