Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static WheelCoveringBuilder.RequirementsControlType |
WheelCoveringBuilder.RequirementsControlType.STANDARD_DRIVEN
Represents the option for reading parameters from the config file
|
static WheelCoveringBuilder.RequirementsControlType |
WheelCoveringBuilder.RequirementsControlType.USER_DEFINED
Represents the option for input of user defined parameters
|
Modifier and Type | Method and Description |
---|---|
WheelCoveringBuilder.RequirementsControlType |
WheelCoveringBuilder.requirementsControl()
Returns the requirements control for standard driven or user defined.
|
static WheelCoveringBuilder.RequirementsControlType |
WheelCoveringBuilder.RequirementsControlType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WheelCoveringBuilder.RequirementsControlType |
WheelCoveringBuilder.RequirementsControlType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WheelCoveringBuilder.RequirementsControlType[] |
WheelCoveringBuilder.RequirementsControlType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WheelCoveringBuilder.setRequirementsControl(WheelCoveringBuilder.RequirementsControlType requirement)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.