Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static WheelCoveringBuilder.PositionType |
WheelCoveringBuilder.PositionType.BOTH
Creates checking surface for both front and rear wheels
|
static WheelCoveringBuilder.PositionType |
WheelCoveringBuilder.PositionType.FRONT
Creates checking surface for front wheel only
|
static WheelCoveringBuilder.PositionType |
WheelCoveringBuilder.PositionType.REAR
Creates checking surface for rear wheel only
|
Modifier and Type | Method and Description |
---|---|
WheelCoveringBuilder.PositionType |
WheelCoveringBuilder.position()
Returns the wheel covering position.
|
static WheelCoveringBuilder.PositionType |
WheelCoveringBuilder.PositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WheelCoveringBuilder.PositionType |
WheelCoveringBuilder.PositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WheelCoveringBuilder.PositionType[] |
WheelCoveringBuilder.PositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WheelCoveringBuilder.setPosition(WheelCoveringBuilder.PositionType position)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.