Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.TireDefinitionOption.PROFILE_CURVES
Use curves in the current work part.
|
static TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.TireDefinitionOption.PROFILE_POINT_FILE
Read a text file with tire profile points.
|
static TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.TireDefinitionOption.SKETCHFROM_OTHER_PART
Use curves from a sketch in another part.
|
static TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.TireDefinitionOption.SOLID_BODY
Use a solid body.
|
Modifier and Type | Method and Description |
---|---|
TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.tireDefinition()
Returns the option to specify the method of tire profile definition.
|
static TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.TireDefinitionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TireEnvelopeBuilder.TireDefinitionOption |
TireEnvelopeBuilder.TireDefinitionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TireEnvelopeBuilder.TireDefinitionOption[] |
TireEnvelopeBuilder.TireDefinitionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TireEnvelopeBuilder.setTireDefinition(TireEnvelopeBuilder.TireDefinitionOption tireDefinition)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.