Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static SeatBeltAnchorageBuilder.SeatTypes |
SeatBeltAnchorageBuilder.SeatTypes.FIXED
fixed
|
static SeatBeltAnchorageBuilder.SeatTypes |
SeatBeltAnchorageBuilder.SeatTypes.MOVABLE_FRONT
front
|
static SeatBeltAnchorageBuilder.SeatTypes |
SeatBeltAnchorageBuilder.SeatTypes.MOVABLE_REAR
rear
|
Modifier and Type | Method and Description |
---|---|
SeatBeltAnchorageBuilder.SeatTypes |
SeatBeltAnchorageBuilder.seatType()
Returns the seat type
License requirements: None. |
static SeatBeltAnchorageBuilder.SeatTypes |
SeatBeltAnchorageBuilder.SeatTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.SeatTypes |
SeatBeltAnchorageBuilder.SeatTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.SeatTypes[] |
SeatBeltAnchorageBuilder.SeatTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SeatBeltAnchorageBuilder.setSeatType(SeatBeltAnchorageBuilder.SeatTypes seatType)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.