Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.ShowVisionConeType.ALL
Represents both of Eye-Mirror and Mirror Target vision cones are shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.ShowVisionConeType.EYE_TO_MIRROR
Represents only Eye-Mirror vision cone is shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.ShowVisionConeType.MIRROR_TO_TARGET
Represents only Mirror-Target vision cone is shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.ShowVisionConeType.NONE
Represents the vision cones aren't shown
|
Modifier and Type | Method and Description |
---|---|
MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.showVisionCone()
Returns the indication if the vision cone is shown.
|
static MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.ShowVisionConeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.ShowVisionConeType |
MirrorCertificationBuilder.ShowVisionConeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.ShowVisionConeType[] |
MirrorCertificationBuilder.ShowVisionConeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorCertificationBuilder.setShowVisionCone(MirrorCertificationBuilder.ShowVisionConeType showVisionCone)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.