Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static GroundClearanceBuilder.SurfaceLengthType |
GroundClearanceBuilder.SurfaceLengthType.FRONT_TO_REAR |
static GroundClearanceBuilder.SurfaceLengthType |
GroundClearanceBuilder.SurfaceLengthType.FULL_VEHICLE |
Modifier and Type | Method and Description |
---|---|
GroundClearanceBuilder.SurfaceLengthType |
GroundClearanceBuilder.surfaceLength()
Returns the surface length type which determines the length of the general surface.
|
static GroundClearanceBuilder.SurfaceLengthType |
GroundClearanceBuilder.SurfaceLengthType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GroundClearanceBuilder.SurfaceLengthType |
GroundClearanceBuilder.SurfaceLengthType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GroundClearanceBuilder.SurfaceLengthType[] |
GroundClearanceBuilder.SurfaceLengthType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GroundClearanceBuilder.setSurfaceLength(GroundClearanceBuilder.SurfaceLengthType surfaceLength)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.