Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static GroundClearanceBuilder.PositionType |
GroundClearanceBuilder.PositionType.BOTH |
static GroundClearanceBuilder.PositionType |
GroundClearanceBuilder.PositionType.FRONT |
static GroundClearanceBuilder.PositionType |
GroundClearanceBuilder.PositionType.REAR |
Modifier and Type | Method and Description |
---|---|
GroundClearanceBuilder.PositionType |
GroundClearanceBuilder.position()
Returns the position of the under axle surface.
|
static GroundClearanceBuilder.PositionType |
GroundClearanceBuilder.PositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GroundClearanceBuilder.PositionType |
GroundClearanceBuilder.PositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GroundClearanceBuilder.PositionType[] |
GroundClearanceBuilder.PositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GroundClearanceBuilder.setPosition(GroundClearanceBuilder.PositionType position)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.