Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static DynamicCurbBuilder.WheelType |
DynamicCurbBuilder.WheelType.DIAMETER |
static DynamicCurbBuilder.WheelType |
DynamicCurbBuilder.WheelType.STATIC_RADIUS |
Modifier and Type | Method and Description |
---|---|
static DynamicCurbBuilder.WheelType |
DynamicCurbBuilder.WheelType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DynamicCurbBuilder.WheelType |
DynamicCurbBuilder.WheelType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DynamicCurbBuilder.WheelType[] |
DynamicCurbBuilder.WheelType.values()
Returns an array that contains the values for this enum.
|
DynamicCurbBuilder.WheelType |
DynamicCurbBuilder.wheelSize()
Returns the wheel size option which determines the size of the wheels in the dynamic curb.
|
Modifier and Type | Method and Description |
---|---|
void |
DynamicCurbBuilder.setWheelSize(DynamicCurbBuilder.WheelType wheelSize)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.