Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static DynamicCurbBuilder.MethodType |
DynamicCurbBuilder.MethodType.HORIZONTAL |
static DynamicCurbBuilder.MethodType |
DynamicCurbBuilder.MethodType.PARALLEL_TANGENT |
static DynamicCurbBuilder.MethodType |
DynamicCurbBuilder.MethodType.VERTICAL_TANGENT |
Modifier and Type | Method and Description |
---|---|
DynamicCurbBuilder.MethodType |
DynamicCurbBuilder.innerLineType()
Returns the inner line type for dynamic curb.
|
static DynamicCurbBuilder.MethodType |
DynamicCurbBuilder.MethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DynamicCurbBuilder.MethodType |
DynamicCurbBuilder.MethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DynamicCurbBuilder.MethodType[] |
DynamicCurbBuilder.MethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DynamicCurbBuilder.setInnerLineType(DynamicCurbBuilder.MethodType innerLineType)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.