Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static CloseRangeVisibilityBuilder.EyePointTypes |
CloseRangeVisibilityBuilder.EyePointTypes.BINOCULAR
Binocular type
|
static CloseRangeVisibilityBuilder.EyePointTypes |
CloseRangeVisibilityBuilder.EyePointTypes.MONOCULAR
Monocular type
|
Modifier and Type | Method and Description |
---|---|
CloseRangeVisibilityBuilder.EyePointTypes |
CloseRangeVisibilityBuilder.eyePointType()
Returns the eye point types to define the close range visibility.
|
static CloseRangeVisibilityBuilder.EyePointTypes |
CloseRangeVisibilityBuilder.EyePointTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CloseRangeVisibilityBuilder.EyePointTypes |
CloseRangeVisibilityBuilder.EyePointTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CloseRangeVisibilityBuilder.EyePointTypes[] |
CloseRangeVisibilityBuilder.EyePointTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CloseRangeVisibilityBuilder.setEyePointType(CloseRangeVisibilityBuilder.EyePointTypes eyePointType)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.