Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static BaseDataWheelBuilder.PositionDefinitionOptions |
BaseDataWheelBuilder.PositionDefinitionOptions.ATTACHMENT_POINT_RIM_OFFSET |
static BaseDataWheelBuilder.PositionDefinitionOptions |
BaseDataWheelBuilder.PositionDefinitionOptions.WHEEL_CENTER_POINT |
Modifier and Type | Method and Description |
---|---|
BaseDataWheelBuilder.PositionDefinitionOptions |
BaseDataWheelBuilder.positionDefinition()
Returns the value to indicate which option is used to define the wheel position.
|
static BaseDataWheelBuilder.PositionDefinitionOptions |
BaseDataWheelBuilder.PositionDefinitionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseDataWheelBuilder.PositionDefinitionOptions |
BaseDataWheelBuilder.PositionDefinitionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseDataWheelBuilder.PositionDefinitionOptions[] |
BaseDataWheelBuilder.PositionDefinitionOptions.values()
Returns an array that contains the values for this enum.
|
BaseDataWheelBuilder.PositionDefinitionOptions |
BaseDataBuilder.wheelPositionDefinition()
Returns the wheel position definition option of the vehicle.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseDataWheelBuilder.setPositionDefinition(BaseDataWheelBuilder.PositionDefinitionOptions positionDefinition)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
BaseDataBuilder.setWheelPositionDefinition(BaseDataWheelBuilder.PositionDefinitionOptions positionDefinition)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.