Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Method and Description |
---|---|
BaseDataPassengerBuilder |
BaseDataBuilder.createPassenger(BaseDataPassengerBuilder pOther)
Creates an instance of
BaseDataPassengerBuilder from another instance. |
BaseDataPassengerBuilder |
BaseDataBuilder.getNthPassenger(int nIndex)
Returns the nth passenger, which represents
BaseDataPassengerBuilder , from the base data. |
BaseDataPassengerBuilder |
BaseDataBuilder.passengerDefinition()
Returns the passenger definition.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseDataBuilder.addPassenger(BaseDataPassengerBuilder passenger)
Adds a passenger, which represents
BaseDataPassengerBuilder , to the base data. |
void |
BaseDataPassengerBuilder.assign(BaseDataPassengerBuilder other)
Assigns values from another passenger.
|
BaseDataPassengerBuilder |
BaseDataBuilder.createPassenger(BaseDataPassengerBuilder pOther)
Creates an instance of
BaseDataPassengerBuilder from another instance. |
void |
BaseDataBuilder.removePassenger(BaseDataPassengerBuilder passenger)
Removes a passenger, which represents
BaseDataPassengerBuilder , from the base data. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.