Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.BACKWARD
Seat position opposite to the driving direction
|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.CUSTOM
Specify a custom value for the seat position (in deg). 1 to 179: Turning the seat rightwards; 1 to 179: Turning the seat leftwards.
|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.FRONTWARD
Seat position driving direction
|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.LEFT
Seat directed towards the left side of the car.
|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.RIGHT
Seat directed towards the right side of the car.
|
Modifier and Type | Method and Description |
---|---|
BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.seatDirection()
Returns the direction that this passenger is facing.
|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseDataPassengerBuilder.SeatDirectionOptions |
BaseDataPassengerBuilder.SeatDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseDataPassengerBuilder.SeatDirectionOptions[] |
BaseDataPassengerBuilder.SeatDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseDataPassengerBuilder.setSeatDirection(BaseDataPassengerBuilder.SeatDirectionOptions seatDirection)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.