Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Method and Description |
---|---|
BaseDataLoadingBuilder |
BaseDataBuilder.createLoading(BaseDataLoadingBuilder pOther)
Creates an instance of
BaseDataLoadingBuilder from another instance. |
BaseDataLoadingBuilder |
BaseDataBuilder.getNthLoading(int nIndex)
Returns the nth loading, which represents
BaseDataLoadingBuilder , from the base data. |
BaseDataLoadingBuilder |
BaseDataBuilder.loadingDefinition()
Returns the loading definition.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseDataBuilder.addLoading(BaseDataLoadingBuilder loading)
Adds a loading, which represents
BaseDataLoadingBuilder , to the base data. |
void |
BaseDataLoadingBuilder.assign(BaseDataLoadingBuilder other)
Assigns value from another loading.
|
BaseDataLoadingBuilder |
BaseDataBuilder.createLoading(BaseDataLoadingBuilder pOther)
Creates an instance of
BaseDataLoadingBuilder from another instance. |
void |
BaseDataBuilder.removeLoading(BaseDataLoadingBuilder loading)
Removes a loading, which represents
BaseDataLoadingBuilder , from the base data. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.