Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static BaseDataLoadingBuilder.LoadingType |
BaseDataLoadingBuilder.LoadingType.STANDARD
Standard - Defined in the registration file, user can not delete it.
|
static BaseDataLoadingBuilder.LoadingType |
BaseDataLoadingBuilder.LoadingType.USER_DEFINED
User-Defined - user can add or delete it.
|
Modifier and Type | Method and Description |
---|---|
BaseDataLoadingBuilder.LoadingType |
BaseDataLoadingBuilder.type()
Returns the vehicle loading type.
|
static BaseDataLoadingBuilder.LoadingType |
BaseDataLoadingBuilder.LoadingType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseDataLoadingBuilder.LoadingType |
BaseDataLoadingBuilder.LoadingType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseDataLoadingBuilder.LoadingType[] |
BaseDataLoadingBuilder.LoadingType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseDataLoadingBuilder.setType(BaseDataLoadingBuilder.LoadingType loadingType)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.