public interface WheelFixingBuilder
WheelFixing
builder used to
create or edit a vehicle design wheel fixing. nxopen.features.vehicledesignCollection#createWheelFixingBuilder
Property | Value |
---|---|
HeightZ.Value | 0 |
LengthX.Value | 0 |
LevelZ.Value | 0 |
ObjectPosition | WheelExtents |
Position | Front |
Radius.Value | 0 |
RequirementsControl | StandardDriven |
Shape | Block |
WheelSize | StaticRadius |
WidthY.Value | 0 |
Modifier and Type | Interface and Description |
---|---|
static class |
WheelFixingBuilder.ObjectPositionType
Represents the object position used to indicate if the wheel fixing is positioned at the theoretically
widest dimension of the wheel (diameter) or exactly at the wheel geometry of the base data.
|
static class |
WheelFixingBuilder.PositionType
Represents the wheel fixing positions.
|
static class |
WheelFixingBuilder.RequirementsControlType
Represents the requirements control types to define the wheel fixing.
|
static class |
WheelFixingBuilder.ShapeType
Represents the shape used to indicate if the wheel fixing is a block or a circle segment.
|
static class |
WheelFixingBuilder.WheelSizeType
Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels.
|
Modifier and Type | Method and Description |
---|---|
Expression |
heightZ()
Returns the expression that contains the value which indicates the height Z of the wheel fixing when the shape is block.
|
Expression |
lengthX()
Returns the expression that contains the value which indicates the Length X of the wheel fixing when the shape is block.
|
Expression |
levelZ()
Returns the expression that contains the value which indicates the level Z of the wheel fixing when the shape is circle segment.
|
String |
loading()
Returns the loading used in the wheel fixing.
|
WheelFixingBuilder.ObjectPositionType |
objectPosition()
Returns the wheel fixing object position.
|
WheelFixingBuilder.PositionType |
position()
Returns the wheel fixing position.
|
Expression |
radius()
Returns the expression that contains the value which indicates the radius of the wheel fixing when the shape is circle segment.
|
WheelFixingBuilder.RequirementsControlType |
requirementsControl()
Returns the requirements control for standard driven or user defined.
|
void |
setLoading(String loading)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
setObjectPosition(WheelFixingBuilder.ObjectPositionType objectPosition)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
setPosition(WheelFixingBuilder.PositionType position)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
setRequirementsControl(WheelFixingBuilder.RequirementsControlType requirementsControl)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
setShape(WheelFixingBuilder.ShapeType shape)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
setStandard(String standard)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
setWheelSize(WheelFixingBuilder.WheelSizeType wheelSize)
License requirements: nx_general_packaging ("NX General Packaging") . |
WheelFixingBuilder.ShapeType |
shape()
Returns the wheel fixing shape.
|
String |
standard()
Returns the standard used to define the wheel fixing.
|
WheelFixingBuilder.WheelSizeType |
wheelSize()
Returns the wheel size of the wheel fixing.
|
Expression |
widthY()
Returns the expression that contains the value which indicates the Width Y of the wheel fixing when the shape is block.
|
WheelFixingBuilder.RequirementsControlType requirementsControl() throws NXException, RemoteException
NXException
RemoteException
void setRequirementsControl(WheelFixingBuilder.RequirementsControlType requirementsControl) throws NXException, RemoteException
requirementsControl
- NXException
RemoteException
String standard() throws NXException, RemoteException
WheelFixingBuilder.RequirementsControlType.STANDARD_DRIVEN
.
NXException
RemoteException
void setStandard(String standard) throws NXException, RemoteException
standard
- NXException
RemoteException
String loading() throws NXException, RemoteException
NXException
RemoteException
void setLoading(String loading) throws NXException, RemoteException
loading
- NXException
RemoteException
WheelFixingBuilder.PositionType position() throws NXException, RemoteException
NXException
RemoteException
void setPosition(WheelFixingBuilder.PositionType position) throws NXException, RemoteException
position
- NXException
RemoteException
WheelFixingBuilder.WheelSizeType wheelSize() throws NXException, RemoteException
NXException
RemoteException
void setWheelSize(WheelFixingBuilder.WheelSizeType wheelSize) throws NXException, RemoteException
wheelSize
- NXException
RemoteException
WheelFixingBuilder.ShapeType shape() throws NXException, RemoteException
NXException
RemoteException
void setShape(WheelFixingBuilder.ShapeType shape) throws NXException, RemoteException
shape
- NXException
RemoteException
Expression levelZ() throws NXException, RemoteException
NXException
RemoteException
Expression radius() throws NXException, RemoteException
NXException
RemoteException
Expression heightZ() throws NXException, RemoteException
NXException
RemoteException
Expression lengthX() throws NXException, RemoteException
NXException
RemoteException
Expression widthY() throws NXException, RemoteException
NXException
RemoteException
WheelFixingBuilder.ObjectPositionType objectPosition() throws NXException, RemoteException
NXException
RemoteException
void setObjectPosition(WheelFixingBuilder.ObjectPositionType objectPosition) throws NXException, RemoteException
objectPosition
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.