public static class TireEnvelopeBuilder.DriverGraphOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BY_SKETCH
Use a sketch to define the driver.
|
static int |
_RECTANGULAR_JOUNCE_REBOUND
Use the rectangular jounce rebound definition.
|
static int |
_RECTANGULAR_TAPERED_X
Use the rectangular definition with taper in the X direction.
|
static int |
_RECTANGULAR_TAPERED_Y
Use the rectangular definition with taper in the Y direction.
|
static int |
_TAPERED_ONE_SIDE
Use the rectangular definition with taper on one side.
|
static int |
_TWO_DRIVERS_ONE_FIXED
Use a fixed definition for two drivers.
|
static TireEnvelopeBuilder.DriverGraphOption |
BY_SKETCH
Use a sketch to define the driver.
|
static TireEnvelopeBuilder.DriverGraphOption |
RECTANGULAR_JOUNCE_REBOUND
Use the rectangular jounce rebound definition.
|
static TireEnvelopeBuilder.DriverGraphOption |
RECTANGULAR_TAPERED_X
Use the rectangular definition with taper in the X direction.
|
static TireEnvelopeBuilder.DriverGraphOption |
RECTANGULAR_TAPERED_Y
Use the rectangular definition with taper in the Y direction.
|
static TireEnvelopeBuilder.DriverGraphOption |
TAPERED_ONE_SIDE
Use the rectangular definition with taper on one side.
|
static TireEnvelopeBuilder.DriverGraphOption |
TWO_DRIVERS_ONE_FIXED
Use a fixed definition for two drivers.
|
Modifier and Type | Method and Description |
---|---|
static TireEnvelopeBuilder.DriverGraphOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TireEnvelopeBuilder.DriverGraphOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TireEnvelopeBuilder.DriverGraphOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final TireEnvelopeBuilder.DriverGraphOption RECTANGULAR_JOUNCE_REBOUND
public static final TireEnvelopeBuilder.DriverGraphOption RECTANGULAR_TAPERED_Y
public static final TireEnvelopeBuilder.DriverGraphOption RECTANGULAR_TAPERED_X
public static final TireEnvelopeBuilder.DriverGraphOption TAPERED_ONE_SIDE
public static final TireEnvelopeBuilder.DriverGraphOption BY_SKETCH
public static final TireEnvelopeBuilder.DriverGraphOption TWO_DRIVERS_ONE_FIXED
public static final int _RECTANGULAR_JOUNCE_REBOUND
public static final int _RECTANGULAR_TAPERED_Y
public static final int _RECTANGULAR_TAPERED_X
public static final int _TAPERED_ONE_SIDE
public static final int _BY_SKETCH
public static final int _TWO_DRIVERS_ONE_FIXED
public static TireEnvelopeBuilder.DriverGraphOption valueOf(int value)
public static TireEnvelopeBuilder.DriverGraphOption valueOf(String name)
public static TireEnvelopeBuilder.DriverGraphOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.