public static class BaseDataWheelBuilder.PositionDefinitionOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ATTACHMENT_POINT_RIM_OFFSET |
static int |
_WHEEL_CENTER_POINT |
static BaseDataWheelBuilder.PositionDefinitionOptions |
ATTACHMENT_POINT_RIM_OFFSET |
static BaseDataWheelBuilder.PositionDefinitionOptions |
WHEEL_CENTER_POINT |
Modifier and Type | Method and Description |
---|---|
static BaseDataWheelBuilder.PositionDefinitionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseDataWheelBuilder.PositionDefinitionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseDataWheelBuilder.PositionDefinitionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BaseDataWheelBuilder.PositionDefinitionOptions WHEEL_CENTER_POINT
public static final BaseDataWheelBuilder.PositionDefinitionOptions ATTACHMENT_POINT_RIM_OFFSET
public static final int _WHEEL_CENTER_POINT
public static final int _ATTACHMENT_POINT_RIM_OFFSET
public static BaseDataWheelBuilder.PositionDefinitionOptions valueOf(int value)
public static BaseDataWheelBuilder.PositionDefinitionOptions valueOf(String name)
public static BaseDataWheelBuilder.PositionDefinitionOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.