public static class SubdivisionProjectCageBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALIGN_NORMAL
Align edges normal to the specified plane
|
static int |
_TO_AVERAGE
Project using best fit plane or axis
|
static int |
_TO_TARGET
Project on target
|
static SubdivisionProjectCageBuilder.Types |
ALIGN_NORMAL
Align edges normal to the specified plane
|
static SubdivisionProjectCageBuilder.Types |
TO_AVERAGE
Project using best fit plane or axis
|
static SubdivisionProjectCageBuilder.Types |
TO_TARGET
Project on target
|
Modifier and Type | Method and Description |
---|---|
static SubdivisionProjectCageBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionProjectCageBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionProjectCageBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final SubdivisionProjectCageBuilder.Types TO_TARGET
public static final SubdivisionProjectCageBuilder.Types TO_AVERAGE
public static final SubdivisionProjectCageBuilder.Types ALIGN_NORMAL
public static final int _TO_TARGET
public static final int _TO_AVERAGE
public static final int _ALIGN_NORMAL
public static SubdivisionProjectCageBuilder.Types valueOf(int value)
public static SubdivisionProjectCageBuilder.Types valueOf(String name)
public static SubdivisionProjectCageBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.