Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.AFT_STBD_OUT_DN
Direction is Aft, Starboard, Outside or Down.
|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.CTR
Thickness is centered about the mold face.
|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.FWD_PORT_IN_UP
Direction is Forward, Port, Inside or Up.
|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.PORT_TO_IN_CTR
Direction is Port, To Reference, Inside or Centered.
|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.STBD_FR_OUT_CTR
Direction is Starboard, From Reference, Outside or Centered.
|
Modifier and Type | Method and Description |
---|---|
ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.thicknessDirection()
Returns the direction in which to apply the thickness.
|
ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.thicknessDirectionOnReference()
Returns the direction in which to apply the thickness when the mold face or grid plane is located on a midship reference.
|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThicknessDirectionBuilder.ThicknessDirectionType |
ThicknessDirectionBuilder.ThicknessDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThicknessDirectionBuilder.ThicknessDirectionType[] |
ThicknessDirectionBuilder.ThicknessDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThicknessDirectionBuilder.setThicknessDirection(ThicknessDirectionBuilder.ThicknessDirectionType thicknessDirection)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
void |
ThicknessDirectionBuilder.setThicknessDirectionOnReference(ThicknessDirectionBuilder.ThicknessDirectionType thicknessDirectionOnReference)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.