Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerSystemBuilder.PointMethods |
StiffenerSystemBuilder.PointMethods.PLANES |
static StiffenerSystemBuilder.PointMethods |
StiffenerSystemBuilder.PointMethods.POINTS |
Modifier and Type | Method and Description |
---|---|
StiffenerSystemBuilder.PointMethods |
StiffenerSystemBuilder.pointMethod()
Returns the method used to define the generated points on the ship structure to define the path of the stiffener system.
|
static StiffenerSystemBuilder.PointMethods |
StiffenerSystemBuilder.PointMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerSystemBuilder.PointMethods |
StiffenerSystemBuilder.PointMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerSystemBuilder.PointMethods[] |
StiffenerSystemBuilder.PointMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StiffenerSystemBuilder.setPointMethod(StiffenerSystemBuilder.PointMethods method)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.