Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerSystemBuilder.OrientationMethods |
StiffenerSystemBuilder.OrientationMethods.FACE_NORMAL |
static StiffenerSystemBuilder.OrientationMethods |
StiffenerSystemBuilder.OrientationMethods.VECTOR |
Modifier and Type | Method and Description |
---|---|
StiffenerSystemBuilder.OrientationMethods |
SubSystemBuilder.orientationMethod()
Returns the method used to define the reference for the orientation angle of stiffener system.
|
StiffenerSystemBuilder.OrientationMethods |
StiffenerSystemBuilder.orientationMethod()
Returns the method used to define the reference for the orientation angle of stiffener system.
|
StiffenerSystemBuilder.OrientationMethods |
EditStockBuilder.orientationMethod()
Deprecated.
Deprecated in NX10.0.0. Orientation method can only be modified on the full profile system itself.
|
static StiffenerSystemBuilder.OrientationMethods |
StiffenerSystemBuilder.OrientationMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerSystemBuilder.OrientationMethods |
StiffenerSystemBuilder.OrientationMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerSystemBuilder.OrientationMethods[] |
StiffenerSystemBuilder.OrientationMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubSystemBuilder.setOrientationMethod(StiffenerSystemBuilder.OrientationMethods orientationMethod)
License requirements: nx_ship_concept ("Ship Concept") . |
void |
StiffenerSystemBuilder.setOrientationMethod(StiffenerSystemBuilder.OrientationMethods orientationMethod)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
EditStockBuilder.setOrientationMethod(StiffenerSystemBuilder.OrientationMethods orientationMethod)
Deprecated.
Deprecated in NX10.0.0. Orientation method can only be modified on the full profile system itself.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.