Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerSystemBuilder.OffsetSpacingModes |
StiffenerSystemBuilder.OffsetSpacingModes.DOUBLE |
static StiffenerSystemBuilder.OffsetSpacingModes |
StiffenerSystemBuilder.OffsetSpacingModes.SINGLE |
Modifier and Type | Method and Description |
---|---|
StiffenerSystemBuilder.OffsetSpacingModes |
StiffenerSystemBuilder.offsetSpacingMode()
Returns the indication whether spacing of the offset planes is defined at each end of the stiffener system,
or if a constant spacing is desired.
|
static StiffenerSystemBuilder.OffsetSpacingModes |
StiffenerSystemBuilder.OffsetSpacingModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerSystemBuilder.OffsetSpacingModes |
StiffenerSystemBuilder.OffsetSpacingModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerSystemBuilder.OffsetSpacingModes[] |
StiffenerSystemBuilder.OffsetSpacingModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StiffenerSystemBuilder.setOffsetSpacingMode(StiffenerSystemBuilder.OffsetSpacingModes offsetSpacingMode)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.