Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
SplitProfilePlateBuilder.SplitDirectionOptionType.ALONG_PLANE_OR_FACE
Split profile/plate along selected plane or face
|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
SplitProfilePlateBuilder.SplitDirectionOptionType.PERPENDICULAR_TO_MOLDING_FACE
create plane/face perpendicular to molding face as the split tool
|
Modifier and Type | Method and Description |
---|---|
SplitProfilePlateBuilder.SplitDirectionOptionType |
SplitProfilePlateBuilder.splitDirectionOption()
Returns the option to split profile/plate along tool face or perpendicular to profile/plate molding face.
|
SplitProfilePlateBuilder.SplitDirectionOptionType |
ShipTrimBodyBuilder.splitDirectionOption()
Returns the split direction method being used to construct the splitting sheet body.
|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
SplitProfilePlateBuilder.SplitDirectionOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplitProfilePlateBuilder.SplitDirectionOptionType |
SplitProfilePlateBuilder.SplitDirectionOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplitProfilePlateBuilder.SplitDirectionOptionType[] |
SplitProfilePlateBuilder.SplitDirectionOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SplitProfilePlateBuilder.setSplitDirectionOption(SplitProfilePlateBuilder.SplitDirectionOptionType splitDirectionOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
void |
ShipTrimBodyBuilder.setSplitDirectionOption(SplitProfilePlateBuilder.SplitDirectionOptionType splitDirectionOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.