Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShipEndCutBuilder.CreationMethod |
ShipEndCutBuilder.CreationMethod.FACE_EDGE
1 face and 1 edge are used to place this endcut
|
static ShipEndCutBuilder.CreationMethod |
ShipEndCutBuilder.CreationMethod.SPECIFY_CSYS
a csys is used to place this endcut
|
Modifier and Type | Method and Description |
---|---|
ShipEndCutBuilder.CreationMethod |
ShipEndCutBuilder.placementType()
Returns the placement type
License requirements: None. |
static ShipEndCutBuilder.CreationMethod |
ShipEndCutBuilder.CreationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipEndCutBuilder.CreationMethod |
ShipEndCutBuilder.CreationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipEndCutBuilder.CreationMethod[] |
ShipEndCutBuilder.CreationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShipEndCutBuilder.setPlacementType(ShipEndCutBuilder.CreationMethod placementType)
License requirements: nx_ship_concept ("Ship Concept") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.