Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SectionDrawingBuilder.SectionsPerDrawingOptions |
SectionDrawingBuilder.SectionsPerDrawingOptions.MULTIPLE |
static SectionDrawingBuilder.SectionsPerDrawingOptions |
SectionDrawingBuilder.SectionsPerDrawingOptions.SINGLE |
Modifier and Type | Method and Description |
---|---|
SectionDrawingBuilder.SectionsPerDrawingOptions |
SectionDrawingBuilder.sectionsPerDrawing()
Returns the sct per drawing
License requirements: None. |
static SectionDrawingBuilder.SectionsPerDrawingOptions |
SectionDrawingBuilder.SectionsPerDrawingOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionDrawingBuilder.SectionsPerDrawingOptions |
SectionDrawingBuilder.SectionsPerDrawingOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionDrawingBuilder.SectionsPerDrawingOptions[] |
SectionDrawingBuilder.SectionsPerDrawingOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionDrawingBuilder.setSectionsPerDrawing(SectionDrawingBuilder.SectionsPerDrawingOptions sctPerDrawing)
License requirements: nx_ship_drafting ("Ship Drafting") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.