Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
SeamBlockBuilder |
BuiltUpBlockBuilder.createSeamBlockBuilder()
Creates a
SeamBlockBuilder
License requirements: None. |
SeamBlockBuilder |
SeamBlockBuilderList.findItem(int index)
Returns the object at the input index.
|
SeamBlockBuilder[] |
SeamBlockBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SeamBlockBuilderList.append(SeamBlockBuilder object)
Appends an object to the list
License requirements: None. |
void |
SeamBlockBuilderList.append(SeamBlockBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SeamBlockBuilderList.erase(SeamBlockBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SeamBlockBuilderList.erase(SeamBlockBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SeamBlockBuilderList.findIndex(SeamBlockBuilder obj)
Finds the index where the input object appears.
|
void |
SeamBlockBuilderList.insert(int location,
SeamBlockBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SeamBlockBuilderList.setContents(SeamBlockBuilder[] objects)
Sets the contents of the entire list.
|
void |
SeamBlockBuilderList.swap(SeamBlockBuilder object1,
SeamBlockBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.